Technical FAQs

Ask a Question

Why does the error output of the MBP_MSTR block come on when the block is not enabled?

The MBP_MSTR block programmed in either Concept or Unity Pro will error if the CONTROL and DATABUF outputs are not located to 4X registers. The ERROR output may come on for a number of reasons, but the ERROR output on without the ENABLE input high indicates that the CONTROL and DATABUF outputs are not located.



Legacy KB System (APS) Data: RESL161452 V2.0, Originally authored by DaSo on 04/01/2009, Last Edited by DaSo on 04/01/2009
Related ranges: Modbus Plus
Was this helpful?
What can we do to improve the information ?