Technical FAQs

Ask a Question

Could ATV31's logic input be defined several functions at same time? For example, ATV31's LI3 is defined as " DC injection stop", "JOG" and " ramp...

Goals and Symptoms

Could ATV31's logic input be defined several functions at same time?

For example, ATV31's LI3 is defined as " DC injection stop", "JOG" and " ramp switchng" at same time. What does ATV31 behave if LI3 is activated at this condition above? What function has the priority? Why?

Causes and Fixes

The philosophy of the ATV31 is multi-affectation of the Li without restriction, so you need to be logic. is it necessary to have " DC injection stop " in the same time " ramps switching " and " JOG ". In your case, the priority order is : Stop, Jog, Ramp.


Legacy KB System (APS) Data: RESL161410 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 31
Was this helpful?
What can we do to improve the information ?