Technical FAQs

Ask a Question

I need to have the mH datas for the motor line chokes of ATV28 and 58 .BR Asli

Goals and Symptoms

I need to have the mH datas for the motor line chokes of ATV28 & 58 .BR Asli

Causes and Fixes

VW3A66501 = 10 mH 4 A
VW3A66502 = 4 mH 10 A
VW3A66503 = 2m H 16 A
VW3A66504 = 1m H 30 A
VW3A66505 = 0,5 mH 60 A
VW3A66506 = 0,3 mH 100 A
VW3A66507 = 0,15 mH 230 A
VW3A66508 = 0,075 mH 370 A
VW3A66509 = 0,050 mH 500 A

Was this helpful?
What can we do to improve the information ?