Technical FAQs

Ask a Question

Would braking resistor get warm even when ATV28 is merely at "rdy" state ? Is it in normal condition? (If braking resistor's specification is well fit...

Goals and Symptoms

Would braking resistor get warm even when ATV28 is merely at "rdy" state ? Is it in normal condition? (If braking resistor's specification is well fitted with its cooperated ATV28, and it is also in good condition without any insulation problem.)

Causes and Fixes

On the ATV28 the braking transistor switch on the resistor following the DC bus value just before Overvoltage fault. But in this case, the network is superior to the limit.


Legacy KB System (APS) Data: RESL161354 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 28
Was this helpful?
What can we do to improve the information ?