Technical FAQs

Ask a Question

Is it possible to read some data like current or speed from an ATV58 via Modbus but to control the ATV I want to use the teminal LI1 at the same time?...

Goals and Symptoms

Is it possible to read some data like current or speed from an ATV58 via Modbus but to control the ATV I want to use the teminal LI1 at the same time?

Facts and Changes

ATV58 Modbus

Causes and Fixes

This operation mode is possible if you don't send the CMD word, that I mean you can use read_parameter instructions to obtain some data from inverter with Li control.


Legacy KB System (APS) Data: RESL161291 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 58
Was this helpful?
What can we do to improve the information ?