Technical FAQs

Ask a Question

What is the default configuration password for the 170ENT11001 Module?

The default configuration password for the 170ENT11001 module is: " httpcfguser " all in lower case. This gets entered into the configuration web page of the Momentum 170ENT11001 module in order to configure the module IP address or configuration for FDR. Please refer to the user manual number 870USE11400. Version 2.0 or greater.


Legacy KB System (APS) Data: RESL161232 V3.0, Originally authored by MiRo on 06/21/2007, Last Edited by MiMe on 06/21/2007
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?