Technical FAQs

Ask a Question

Zelio2 S2003 vB. Application timer and clock

Goals and Symptoms

Is it possible to have a remote adjustment function of the internal timer with a potentiometer?
The potentiometer connected to the analog input (0-10V) and some FBD timer function that works with the analog input.

Facts and Changes

timer
clock

Causes and Fixes

Yes it is possible, see the attachments, there are 4 examples

Attachments

(Removed File URL: 161227_4FEE/Zelio2_S2003_vC_Timer_&_Clock.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/84130d56b6781fbfc1257363004213a8/fl_block_5/0.56A?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL161227 V5.0, Originally authored by JaLa on 09/27/2007, Last Edited by CyVi on 09/27/2007
Related ranges: Zelio Logic
Was this helpful?
What can we do to improve the information ?