Technical FAQs

Ask a Question

Is it possible to supply, regardless of how the connections to the drive are realised, to power the electronics of all the ATV38/58-range with VW3A586...

Goals and Symptoms

Is it possible to supply, regardless of how the connections to the drive are realised, to power the electronics of all the ATV38/58-range with VW3A58604 ? In this case ATV38HC13N4X is interesting (Profibus- communication).

Facts and Changes

ATV38 and VW3A58604

Causes and Fixes

It's possible and two ways:

- for size <= 15 kw follow the instructions sheet.
- for size > 15 kw follow the Attached document, to resume it's necessary to supply the control board 1 sec before the power ( for the first time ) and after that it's possible to have the control board powered permanently.
 

Attachments

(Removed File URL: 161212_4FD6/ATV58_diagram_of_separate_supply_VW3A58602_4_n.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/a2e055ec3a2f7e6985256ea900443c6b/fl_block_5/0.680?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL161212 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 38
Was this helpful?
What can we do to improve the information ?