Technical FAQs

Ask a Question

Is it possible to supply, regardless of how the connections to the drive are realised, to power the electronics of all the ATV38/58-range with VW3A586...

Goals and Symptoms

Is it possible to supply, regardless of how the connections to the drive are realised, to power the electronics of all the ATV38/58-range with VW3A58604 ? In this case ATV38HC13N4X is interesting (Profibus- communication).

Facts and Changes

ATV38 and VW3A58604

Causes and Fixes

It's possible and two ways:

- for size <= 15 kw follow the instructions sheet.
- for size > 15 kw follow the Attached document, to resume it's necessary to supply the control board 1 sec before the power ( for the first time ) and after that it's possible to have the control board powered permanently.

Attachments

(Removed File URL: 161209_4FCA/ATV58_alimentation_separ_C3_A9e_adaptation_pour_Minerve.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/7532379f651f9c4185256e6f00334450/fl_block_5/0.68C?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL161209 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 38
Was this helpful?
What can we do to improve the information ?