Technical FAQs

Ask a Question

Why does the alarm remain flashing red in the Alarm History page even though it has been acknowledged on Magelis XBT-F operator interface terminals?


In the history page, you are looking at all of the events of all alarms. The flashing red alarm banner is showing the history of the alarm's occurrence, as well as the occurrence of the alarm being acknowledged.


Legacy KB System (APS) Data: RESL1610 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT-F, TXBT-F
Was this helpful?
What can we do to improve the information ?