Technical FAQs

Ask a Question

How do you start a Compact 984 PLC in "Optimized Mode" using ProWORX Nxt?

You simply select "Optimized Mode" before you start the Compact 984 PLC. To start the Compact 984 PLC in this mode, discrete points are not allowed to be disabled. Also, power flow is not displayed when online with the Compact 984 PLC that is in "Optimized Mode".


Legacy KB System (APS) Data: RESL160972 V1.0, Originally authored by on , Last Edited by on
Related ranges: Compact
Was this helpful?
What can we do to improve the information ?