Technical FAQs

Ask a Question

Can 500 Series I/O be used with a Quantum PLC?

Yes, 500 Series I/O can be use with a Quantum PLC as a Remote I/O drop. To make the 500 Series I/O a Remote I/O drop, you will need to purchase and incorporate the following parts into the system:
1. An AS-P451-xxx with S908 Remote I/O Interface (this will be your Remote I/O drop).
2. An AS-J540-100 200 Series I/O to 500 Series I/O adapter (this will be your I/O bus converter).

Please check on the availability of each prior to committing to this migration strategy.


Legacy KB System (APS) Data: RESL160933 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?