Technical FAQs

Ask a Question

There is a problem with the ATV31 internal supply, its not protected against short circuits between +10V and com! Display is dark. Then display shows ...

Goals and Symptoms

There is a problem with the ATV31 internal supply, its not protected against short circuits between +10V and com! Display is dark. Then display shows inf. Reset only with main supply off! +24V is protected!

Facts and Changes

ATV31

Causes and Fixes

We known this " problem " but unfortunatelly no evolution forecast for this moment.


Legacy KB System (APS) Data: RESL160899 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 31
Was this helpful?
What can we do to improve the information ?