Technical FAQs

Ask a Question

How can I get registers to go over 9999 counts in the ProWorx Plus software?

This is a preference selection in the ProWorx Plus software. From the ProWorx Plus Off-line Main Menu, select "Utilities", "Configuration" and "System Options". From the Systems Options page can then change the "Maximum Decimal Value" from 9999 to 65535 counts.

Was this helpful?
What can we do to improve the information ?