Technical FAQs

Ask a Question

What kind of machine application will require "CLI" current limitation? What kind of machine application will require "tLI" torque limitation?

Goals and Symptoms

What kind of machine application will require "CLI" current limitation? What kind of machine application will require "tLI" torque limitation?

Causes and Fixes

CLI used for :
extruding
pumping
where the motor is working as a generator
hoisting
lift
crimp stamp

TLI:
ss applications to limit the applied torque to prevent mechanical problems, you can also use it to check if the rotor is lock. The second torque limitation is available to limit the torque at the starting time and after during the normal operation. In a normal way there is a nominal torque for normal speed, if there is some variations you need to use the 58F ( roller-deroulor ). And you can use the current limitation if there is no torque limitation or in case of generator mode to limit the max value provide by the inverter to protect it.

Winding
Unwinding

Was this helpful?
What can we do to improve the information ?