Technical FAQs

Ask a Question

Are there any data of speed precision for the ATV31-range. Need data to compare with ABB-drives. Is ATV31 competitive with ABB-drives with their DTC ...

Goals and Symptoms

Are there any data of speed precision for the ATV31-range. Need data to compare with ABB-drives. Is ATV31 competitive with ABB-drives with their DTC (direct torque control)-system ?

Facts and Changes

ATV31H...N4, 0,37 to 5,5kW, speed precision.

Causes and Fixes

It's the same like ATV58 in open loop, it's +/- 1%


Legacy KB System (APS) Data: RESL160825 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 31
Was this helpful?
What can we do to improve the information ?