Technical FAQs

Ask a Question

Are the connectors included when ordering Advantys STB IO modules?

No, the connectors have to be ordered separately depending on the module type and connection type (screw or spring). The connectors are sold in lots of 20.

Type
For I/O Modules
Part Number
Screw-type
STBDDI
STBDDO
STBXTS1100
Spring-type
STBDDI
STBDDO
STBXTS2100
Screw-type
STBDAI
STBDAO
STBDRC
STBDRA
STBXTS1110
Spring-type
STBDAI
STBDAO
STBDRC
STBDRA
STBXTS2110
Please refer to the Advantys STB catalog for additional information.

Legacy KB System (APS) Data: RESL160765 V2.0, Originally authored by on , Last Edited by on
Related ranges: Advantys STB
Was this helpful?
What can we do to improve the information ?