Technical FAQs

Ask a Question

Can the Modbus port / ports on the Compact 984 be configured for RS485 mode?

No, the Compact 984 Modbus port / ports cannot be configured for RS485 mode. If this type of communications is needed, you need to use a RS232/RS485 converter that is externally powered.


Legacy KB System (APS) Data: RESL160627 V1.0, Originally authored by on , Last Edited by on
Related ranges: Compact
Was this helpful?
What can we do to improve the information ?