Technical FAQs

Ask a Question

What is the maximum length of cable for an RS485 network when talking to a Momentum PLC?

When communicating with a Momentum PLC the maximum length of cable from one end of the Modbus RS485 network to another is 2000 feet (609m).

Was this helpful?
What can we do to improve the information ?