Technical FAQs

Ask a Question

Are the connectors included when ordering Advantys PDT power distribution modules?

No, the connectors have to be ordered separately. The connectors are sold in lots of 10. For screw type connectors, order STBXTS1130 and for spring type order STBXTS2130.


Legacy KB System (APS) Data: RESL160503 V2.0, Originally authored by on , Last Edited by on
Related ranges: Advantys STB
Was this helpful?
What can we do to improve the information ?