Technical FAQs

Ask a Question

Can I install my copper Modbus Plus network in a star topology?

No. Modbus Plus copper networks cannot be installed in a star topology. The only legal Modbus Plus copper network topology is a linear topology..

Legacy KB System (APS) Data: RESL160499 V2.0, Originally authored by PeZa on 04/06/2010, Last Edited by MiOB on 04/06/2010
Related ranges: Modbus Plus
Was this helpful?
What can we do to improve the information ?