Technical FAQs

Ask a Question

Can I use more than one Momentum Option Adapter with my M1 processor?

No. Only one Momentum Option Adapter per CPU can be used.


Legacy KB System (APS) Data: RESL160498 V2.0, Originally authored by PeZa on 04/04/2009, Last Edited by RoAl on 04/04/2009
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?