Technical FAQs

Ask a Question

ATV31 K protection IP ?

Goals and Symptoms

ATV31 K protection IP ?

Causes and Fixes

ATV31 K is IP55 when mounted in cabinet with seals included with the kit.
See the extract of the catalogue in attachments.
ATV31_kit IP55 from catalogue.zip


Legacy KB System (APS) Data: RESL160478 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 31
Was this helpful?
What can we do to improve the information ?