Technical FAQs

Ask a Question

Can I flash the exec firmware into my PC-E984-X8X PLC using the ProWORX Nxt EXECLoader Wizard?

The ProWORX Nxt EXECLoader Wizard is the same EXECLoader Wizard that Concept uses and it does not support the PC-E984-X8X PLC. The only way to flash the is to do the following;
1. Open ProWORX Nxt
2. Go to the controller tab and select EXECUTIVE FLASH
3. You will then select Write, and then browse to where the source of the exec firmware is and the destination address of the target PLC.

You will now be able to flash the PLC.


Legacy KB System (APS) Data: RESL160404 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?