Technical FAQs

Ask a Question

Can the LUFP9 Devicenet to Modbus gateway be used with the ATS46 softstart. Are EDS files needed for the ATS46 to communicate using this LUfP9.

Goals and Symptoms

Can the LUFP9 Devicenet to Modbus gateway be used with the ATS46 softstart. Are EDS files needed for the ATS46 to communicate using this LUfP9.

Facts and Changes

ATS46, LUFP9

Causes and Fixes

It's possibe to control ATS46 with this gateway with modbus option communication for ATS46. The necessary EDS file is use for the gateway and only for it. You will find all necessary documents in our Lotus Notes database.


Legacy KB System (APS) Data: RESL160225 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 46
Was this helpful?
What can we do to improve the information ?