Technical FAQs

Ask a Question

Can I use an additional keyboard and mouse with my Magelis IPC while the front panel is attached?

Yes, a mouse and keyboard may be added to the Magelis IPC in addition to the ones provided on the front panel. However, these devices cannot be connected via the PS/2 ports on the control box itself. One PS/2 device can be connected on the front panel, the other device will have to be either USB or a DB9 serial device and may be added to the appropriate port on the control box.


Legacy KB System (APS) Data: RESL160105 V2.0, Originally authored by DaSo on 04/05/2012, Last Edited by MiOB on 04/05/2012
Related ranges: Magelis Modular iPC
Was this helpful?
What can we do to improve the information ?