Technical FAQs

Ask a Question

ATV28 Menu is locked from the front panel? Already tried to enter 6969 and 0 for password unlock, but won't work. The keypad is always locked. Only ac...

Goals and Symptoms

ATV28 Menu is locked from the front panel? Already tried to enter 6969 and 0 for password unlock, but won't work. The keypad is always locked. Only access to the drive is through PowerSuite or Remote Keypad Vw3a28101.

Causes and Fixes

Please retry it with a pressure of 2 sec on the Enter key but there is also a bug with the versions before v1.1 ie12.


Legacy KB System (APS) Data: RESL159990 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 28
Was this helpful?
What can we do to improve the information ?