Technical FAQs

Ask a Question

Is there any difference of Pin-out cables for Power Suite PC and Remote Display for ATV18 / ATV28 / ATV31 ? I am asking because we have one costumer t...

Goals and Symptoms

Is there any difference of Pin-out cables for Power Suite PC and Remote Display for ATV18 / ATV28 / ATV31 ? I am asking because we have one costumer that is changing his ATV18 with remote display by ATV´s 28 and in a near future by ATV31, so does the PIN-out and remote displays are compatible by each others?

Facts and Changes

ATV18 / ATV28 / ATV31

Causes and Fixes

The pin-out is the same between ATV 28 ( manufactured since Sept 2001 ) and ATV31, but the keypad are not compatible, not the same software.


Legacy KB System (APS) Data: RESL159962 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 18
Was this helpful?
What can we do to improve the information ?