Technical FAQs

Ask a Question

communcation on Modbus with ATS46 We have a site comprising several ATS46s communicating with TSX Premium master. The communication prot...

Goals and Symptoms

communcation on Modbus with aTS46 We have a site comprising several ATS46s communicating with TSX Premium master. The communication protocol is unitelway.But one of the ATS46s has failed and we have to replace it by a ATS48.But ATS48s only communicate via modbus which means that we need to change communication protocol of other ATS46s with modbus.So,my question is,how can we change the com. protocol of ATS46 from unitelway to modbus?Do we need the ATS software or the panel is sufficient? Or does it recognize the protocol automatically? Best Regards,

Facts and Changes

communcation on Modbus with ATS46

Causes and Fixes

For that you need to have the VW3G46301 option ( normally you have it ) and a PC with Terminal emulation software ( TTY ), included in Windows and also the cable for ATS PC Software and send special request to the ATS, complete procedure in the user's manual page 69 but the best way is to use the PC software ( more simple ). Concerning the physical layer, it's the same.


Legacy KB System (APS) Data: RESL159874 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 46
Was this helpful?
What can we do to improve the information ?