Technical FAQs

Ask a Question

Please advise resolution (how many bits) are the 4 digit, 7 segment display for XUD range. Customer asking for the accuracy of the display.

Goals and Symptoms

Please advise resolution (how many bits) are the 4 digit, 7 segment display for XUD range. Customer asking for the accuracy of the display.

Facts and Changes

XUD
display accuracy

Causes and Fixes

The 7 segment display for XUD range gives an indication about the quantity of light which is received by the PSD, on 16 bits, using a A/N converter from 0 to 4096.
This internal accessory is not an accurate measurement device, but only a kind of VU-meter with the same function as a bar-graph in a consumer product.


Legacy KB System (APS) Data: RESL159827 V1.0, Originally authored by on , Last Edited by on
Related ranges: Osiris
Was this helpful?
What can we do to improve the information ?