Technical FAQs

Ask a Question

If VW3A28100 is used , can we disable it and control Running and stopping the drive by LI1,LI2 and using Potansiometer.

Goals and Symptoms

If VW3A28100 is used , can we disable it and control Running and stopping the drive by LI1,LI2 and using Potansiometer.

Facts and Changes

VW3A28100

Causes and Fixes

If this option is plug there no possibility to control the inverter by the Li.


Legacy KB System (APS) Data: RESL159717 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 28
Was this helpful?
What can we do to improve the information ?