Technical FAQs

Ask a Question

Which memory cards are compatible with the TFTX117 Hand held programmer?

The following cards are for use with the TFTX117 Hand held programmer:
TFTXREM3216 - EEPROM 32K words
TFTXRSM3216 - Protected RAM 32K words
TFTXRSM12816 - Protected RAM 32K words


Legacy KB System (APS) Data: RESL159637 V1.0, Originally authored by on , Last Edited by on
Related ranges: Other HMI
Was this helpful?
What can we do to improve the information ?