Technical FAQs

Ask a Question

Do you have any application example for wireless Modbus communication between ATV58 and Premium PLC (radio, bluetooth etc.)? We need solution for harb...

Goals and Symptoms

Do you have any application example for wireless Modbus communication between ATV58 and Premium PLC (radio, bluetooth etc.)? We need solution for harbor crane which has fixed and rotating part (see picture attached).

Facts and Changes

ATV58

Causes and Fixes

Bluetooth is forecast for next July ( 2004 ) but it's possible with Modbus radio modem. A good provider and more information at: http://www.acromag.com/models.cfm?Product_Function_ID=41&Category_ID=13&Group_ID=2

But we don't have any sample here.

Nota : there is no picture attached

Was this helpful?
What can we do to improve the information ?