Technical FAQs

Ask a Question

What is the suitable action to replace the an ATV66FC10N4 with the new ATV68FC10N4? you have to note the following: 1-ATV 66 is connected to a PLC wi...

Goals and Symptoms

What is the suitable action to replace the an ATV66FC10N4 with the new ATV68FC10N4? you have to note the following:
1-ATV 66 is connected to a PLC with fipway communication
2-how the maintaining on the panel will be
3-the motor was the old one come with ATV66 ,will we make any modifications? the big issue is the communication between drive and PLC as this ATV68 will be spare now and must be ready to be installed at any time

Facts and Changes

ATV66 replacement

Causes and Fixes

Concerning the communication with Fipio you need to add a gateway, VW3A68301 ( you can download the documentation on Intranet at the Shopping kiosk ) , after you need to configure the ATV68 following the application, be careful there is no complete messaging capacity.
No problem for the ATV68 choice. Mechanically these inverters are completly different and you need to adapt some parts ( cables and so on ...).
For the encoder, it's the same ( RS422 - 5v ). Normally it's not necessary to modify the motor.


Legacy KB System (APS) Data: RESL159598 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 68
Was this helpful?
What can we do to improve the information ?