Technical FAQs

Ask a Question

Can ATV38 be used on a 480v supply (US) as an alternative to ATV58?

Goals and Symptoms

Can ATV38 be used on a 480v supply (US) as an alternative to ATV58?

Facts and Changes

ATV38 and suppy 480vac

Causes and Fixes

It depend to the application, what is ?? don't forget the ATV38 is variable torque.
In your case it'a a fan application and there is no problem to use ATV38 as an ATV58.


Legacy KB System (APS) Data: RESL159550 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 38
Was this helpful?
What can we do to improve the information ?