Technical FAQs

Ask a Question

What is the specification for the TSXCSA100/200/500 cable?

The specification for the TSXCSA100/200/500 cable is:
Double twisted pair 24awg
85 ohm /km
shield 12 ohm/km
cap 100 pf /meter
impedance 85ohms
attenuation 13 db/km 0 to 20 kh
max bus 1 km
PE jacket 9.65 mm dia
Belden equivalent 9842


Legacy KB System (APS) Data: RESL159475 V2.0, Originally authored by GeMc on 04/07/2009, Last Edited by GeMc on 04/07/2009
Related ranges: Uni-Telway
Was this helpful?
What can we do to improve the information ?