Technical FAQs

Ask a Question

What is the minimum parameters (technical: RAM, HD, Win...) of computer and PC pocket for instalation of Eco 8 ver. 2.0 and Power Suite programme?

Goals and Symptoms

What is the minimum parameters (technical: RAM, HD, Win...) of computer and PC pocket for instalation of Eco 8 ver. 2.0 and Power Suite programme?

Facts and Changes

Eco 8 Power Suite

Causes and Fixes

PC :
Microsoft Windows® 95 OSR2-98 SE, Microsoft Windows® NT4.X SP5, Microsoft Windows® Me, Microsoft Windows® 2000, Microsoft Windows® XP,
Pentium III, 800 MHz, hard disk 300 Mo free space, 128 Mo RAM,

Pocket PC :
Pocket PC 2002
Processor type ARM or XSCALE, example:

Hewlett Packard® Jornada série 560,
Compaq® IPAQ séries 3800 et 3900.


Legacy KB System (APS) Data: RESL159463 V1.0, Originally authored by on , Last Edited by on
Related ranges: Other VVD PRODUCTS
Was this helpful?
What can we do to improve the information ?