Technical FAQs

Ask a Question

We are looking for the Minimum and Maximun current that require for the XBTN 200 and 400 at pin 7 and 8.

Goals and Symptoms

We are looking for the Minimum and Maximun current that require for the XBTN 200 and 400 at pin 7 and 8.

Facts and Changes

xbtn
power supply

Causes and Fixes

To power up a XBTN2/400, the characteristics are: 5V +/- 5% . 200mA.
Exemple of connections see attached file:

Attachments

(Removed File URL: 159422_3FDA/Connection_XBTN_PC.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/4e1852154373b1fa85256e5900568c79/fl_block_5/0.13BC?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL159422 V2.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT-N
Was this helpful?
What can we do to improve the information ?