Technical FAQs

Ask a Question

How do I import program sections in Unity?

Go to the project browser and choose the task into which you want to import the section. Right click on the sections folder under that task and choose Import as shown below:
..
The Import window will pop up allowing you to navigate to the location of your target section as shown below:
..
Make sure that you have the correct file type selected for the type of section you want to import. Navigate to the location of the exported section, highlight the file and choose <Import>.


Legacy KB System (APS) Data: RESL159421 V3.0, Originally authored by RiVe on 05/13/2010, Last Edited by DaSo on 05/13/2010
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?