Technical FAQs

Ask a Question

PowerSuite Software V1.50 CD contains files for the LUFP7 gateway with the following file extensions: .cfg, .pb, .stx, .gsd, and a couple of Speed...

Goals and Symptoms

PowerSuite Software V1.50 CD contains files for the LUFP7 gateway with the following file extensions: .cfg, .pb, .stx, .gsd, and a couple of Speed Dial files. What application programs are required to open up these files?

Causes and Fixes

.cfg used by ABC Configurator ( gateway )
.pb used by the Profibus configurator ( ie Hilscher )
.stx used by PL7 Pro ( sample on Premium PLC )
.gsd is the file contains Profibus capacities ( used by Hilscher )
Speed Dial files used by ABC Configurator.


Legacy KB System (APS) Data: RESL159378 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 48
Was this helpful?
What can we do to improve the information ?