Technical FAQs

Ask a Question

Is there support for redundant cable Modbus Plus networks within the Magelis HMI product offering?


No, there is no support for redundant cable Modbus Plus networks within the Magelis HMI product offering. XBTF Magelis units can, however, support a single cable Modbus Plus network via usage of the TSXMBP100 interface card.

In addition, The XBTGT, XBTGK and the XBTGW HMI series support a single Modbus Plus network connection via the TSXCUSBMBP gateway or the XBTZGUMP gateway.


Legacy KB System (APS) Data: RESL159118 V2.0, Originally authored by MiMa on 04/04/2009, Last Edited by RoAl on 04/04/2009
Related ranges: Magelis XBT F, TXBT F
Was this helpful?
What can we do to improve the information ?