Technical FAQs

Ask a Question

What is the difference between XUZB01 and XUZB11. Can be used XUZB11 in reflex system (not polarised).

Goals and Symptoms

What is the difference between XUZB01 and XUZB11. Can be used XUZB11 in reflex system (not polarised).

Facts and Changes

XUZB11, XUZB01

Causes and Fixes

XUZB01 is the general purpose adhesive reflector
XUZB11 is dedicated to polarized reflex system.
But it is possible to use XUZB11 with a standard reflex system (not polarized). There is no loss of characteristics. The only condition is to have the same reflective surface.


Legacy KB System (APS) Data: RESL159068 V1.0, Originally authored by on , Last Edited by on
Related ranges: Osiris
Was this helpful?
What can we do to improve the information ?