Technical FAQs

Ask a Question

Are Cablefast or Telefast terminal blocks compatible with other PRODUCTS?

Cablefast terminal blocks are used exclusively with the Quantum I/O family. Telefast terminal blocks used with Telemecanique PRODUCTS are also compatible with vendors such as Siemens and Allen Bradley . Additional details can be found in the following manual " Telefast 2 Prewired System ABE7 " part number # 8501CT9801R2/02.


Legacy KB System (APS) Data: RESL158956 V1.0, Originally authored by on , Last Edited by on
Related ranges: Other Enclosures
Was this helpful?
What can we do to improve the information ?