Technical FAQs

Ask a Question

Do Quantum controllers support DNP3.0 (Distributed Network Protocol) over Ethernet?


There are currently no Schneider Electric PRODUCTS that support DNP3.0 over Ethernet for the Quantum product line.
However there is a third party product available from Prosoft Technologies.
Schneider Electric has not done any official testing on this product.
All testing is performed by Prosoft Technologies.
Therefore, you must contact Prosoft Technologies for support and information on their product.

Legacy KB System (APS) Data: RESL158844 V4.0, Originally authored by MiMa on 04/06/2009, Last Edited by MiMe on 10/10/2009
Related ranges: ConneXium - Ethernet
Was this helpful?
What can we do to improve the information ?