Technical FAQs

Ask a Question

Is possible run Power Suite 1,5 on a HP iPAQ H1915 Pocket PC in Español? Because HP jornada is no available to buy.

Goals and Symptoms

Is possible run Power Suite 1,5 on a HP iPAQ H1915 Pocket PC in Español? Because HP jornada is no available to buy.

Causes and Fixes

Powersuite v1.5 doesn't work directly on H1915 because it's only USB connector, you need to add a RS232 option ( Compaqflash or so on ).


Legacy KB System (APS) Data: RESL158662 V1.0, Originally authored by on , Last Edited by on
Related ranges: Other VVD PRODUCTS
Was this helpful?
What can we do to improve the information ?