Technical FAQs

Ask a Question

For ATV38, Can we use more 2 extentions ? e.g one is I/O extension card and the other one is Device Net comm. card since the price of device net gatea...

Goals and Symptoms

For ATV38, Can we use more 2 extentions ? e.g one is I/O extension card and the other one is Device Net comm. card since the price of device net gateaway is 3 times compare with Device Net comm card.

Facts and Changes

Extention card

Causes and Fixes

It's not possible to put 2 extensions cards on ATV38 ( equal to ATV58 ), you can use a DeviceNet gateway or I/O on DeviceNet.


Legacy KB System (APS) Data: RESL158660 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 38
Was this helpful?
What can we do to improve the information ?