Technical FAQs

Ask a Question

Can the LH4N125RT7 be used with a motor that has a continuous current rating of 25 amps? If so, why does the catalog say the starter has a current ra...

Goals and Symptoms

Can the LH4N125RT7 be used with a motor that has a continuous current rating of 25 amps? If so, why does the catalog say the starter has a current rating of 22 amps? If not, why is the number 25 in the catalog number? Can you send a copy of VVD Info 93?

Facts and Changes

LH4N*25**7 22 or 25 amps?

Causes and Fixes

In fact, 25A is the thermal current ( Ith ) and 22A is the nominal current.

Was this helpful?
What can we do to improve the information ?