Technical FAQs

Ask a Question

What does the termination A27 of the drive ATV68E5C43N4A27 means? There are many references in the Pricat/Prodat that we dont know what it is. For exa...

Goals and Symptoms

What does the termination A27 of the drive ATV68E5C43N4A27 means? There are many references in the Pricat/Prodat that we dont know what it is. For example other references: ATV68E5C10N4A23 ATV68E5C10N4A32 ATV68E5C13N4A24 ATV68E5C15N4A25 ATV68E5C19N4A14 ATV68E5C19N4A26 ATV68E5C23N4A22 ATV68E5C28N4A31 ATV68E5C43N4A27 ATV68E5C53N4A26 ATV68E5C53N4A28 ATV68E5C63N4A40 So what does the termination AXX mean for this cases of the ATV68E5?

Facts and Changes

ATV68E5

Causes and Fixes

The termination A27 and the others are for ATV68 in enclosure for specific customers. You can't order it or if the order come from Renault.


Legacy KB System (APS) Data: RESL157635 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 68
Was this helpful?
What can we do to improve the information ?