Technical FAQs

Ask a Question

For ATV68:- 1. Other than the VW3-A68800(PT Remote mounting kit),can the orginal display and keypad move to other panel through the extension cable? ...

Goals and Symptoms

For ATV68:-
1. Other than the VW3-A68800(PT Remote mounting kit),can the orginal display & keypad move to other panel through the extension cable?
2. can you tell me the line reactor and motor choke is connected in series or in parallel, Refer to cat. no.: VVDED299083EN, Page 30.

Causes and Fixes

1 - This kit is plugged on the RJ45, it's a copy ( functionnality ) of the original keypad.
2 - It's not possible to realize yourself the line reactor and motor choke because there is special elements.


Legacy KB System (APS) Data: RESL157624 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 68
Was this helpful?
What can we do to improve the information ?