Technical FAQs

Ask a Question

Is there any restriction on the cable length between ATV68 brake units and resistors? If yes,what is the value of the cable length for VW3-A687537 ...

Goals and Symptoms

Is there any restriction on the cable length between ATV68 brake units and resistors?

If yes,what is the value of the cable length for VW3-A687537 and VW3-A687537?

Causes and Fixes

The max cable lenght is 10 meters


Legacy KB System (APS) Data: RESL157623 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 68
Was this helpful?
What can we do to improve the information ?